I've designed a LiPo battery charger based on the bq24618 datasheet typical circuit, Fig 19. And am seeing a discrepancy between the datasheet and the EVM doc in terms of whether IC pins are tied to analog or digital ground.
bq24618 datasheet Rev B SLUSA55B Oct 1010 Revised 2015, Fig 19
Connected to analog ground
ACP C2
ISET/ACSET bottom of resistor networks
VREF CE C4
TS C1, R10
Gnd – EP
TTC CTTC
VFB R1
SRP C10
VCC C7
EVM datasheet for bq2461X, SLUU396A Jan 2010 Revised July 2019
Connected to digital ground
ACN C9
ACP C5
ISET/ACSET bottom of resistor networks tied to voltages
VREF C6
TS
VFB R28
VCC C12
SRP C17
SRN C21
only Gnd is connected to analog ground?
Which is correct?