This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: It appears the chip can occasionally start in a fault condition resulting in a high current shoot through or short.

Part Number: LM5175

LM5175 Our application circuit is mostly lifted from the application in the data sheet. In this application, a FET transistor switches power from the rest of the system to the regulator. The fault condition appears to be related to having a very fast turn on of the power source to 28VDC. As yet, we have not been able to capture an event when instrumented likely due to the effect of probes slowing the rise time. Our system applies 22 to 32 VDC to the DC-DC system and when the fault occurs, the power draw is very high for a sustained time until something in the system breaks. If the lab power supply is large enough, the system fuse will blow. If not, then the lab supply will limit current by dropping voltage destroying the FET that switches power to the DC-DC converter.

For this fault to occur, something in the LM5175 logic would have the enable the wrong FETs establishing either a direct path from VIN to return. Is there internal logic reset circuits that could be tripped up by a fast rising VIN?

  • Have you ever tested our EVM? Although you based your design on the schematic shown in the datasheet, we still want to see your own schematic, and please have the component values and part number accurately labeled.

    Thanks,