Other Parts Discussed in Thread: TPS61500
Hello,
i need a driver just like the LM3410, but with a higher switch current.
I want to drive a 10W LED (measured: 9,8V / 1A) with a single 18650 cell.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Carsten,
I am not aware of a device like the LM3410 with a higher current limit. But there is another group within TI that does more low input voltage LED drivers. I will forward this to somebody in that group in case they have something that may be a fit.
Regards,
Clint
Hello Carsten,
I received a reply from somebody else and they recommended the TPS61500. It has a low minimum input voltage and a higher switch current limit. If you are interested and need any support you can post in the LED forum with that part number and the correct person can help you. Thanks.
Regards,
Clint