I have an application using LM5001-Q1 to generate 60V out of 12V and need to deduce the current in 60V power rail from 12V input.
I measured the 12V power rail current before and after I applied the load and the difference is 240uA(15.465mA-15.225mA), which means the load at 60V consumes 48uA assuming 100% efficiency. But when I measure the 60V current directly, it is 51uA.
This is strange, because this indicates the boost's efficiency is more than 100%.
So is the boost itself consumes power differently before and after adding 50uA load on the 60V power rail?