Hi,
I am using the BQ34z100-g1 to estimate SoC of an 8s LiFePO4. As the gauge is not installed as a pack side gauge, it can lose power very occasionally (once in 6 months).
After recovering power supply and with the battery relaxed I send an enable IT command to the gauge to estimate SoC beacuse it restarts with a senseless SoC. I have some questions about this procedure.
1. What is this estimation based on? OCVoltage?
2. if so, where this relation OCV-SoC come from? from the ChemID file? or from data obtained in the learning cycles?
3. What error can I hope in this first estimation with LIFePo4 batterys (where the curve OCV-SoC is very flat)?
4. Is this relation OCV-SoC taking into account the temperature of the battery?
Thank you very much in advance,