Other Parts Discussed in Thread: CSD13381F4, TIDA-00449, CSD13383F4
Hi,
in slua749a, section 4: Cell Balance, it says "A FET with a defined RDS(ON) at approximately ½ the cell voltage is desired."
What does this mean? Should the value of RDS(ON) be half the cell voltage, e.g. 4.2 V -> 2.1 Ohm? Or should half the voltage drop at the FET? I am confused, because I looked at FETs of other designs and the RDS(ON) seemed randomly selected.