Other Parts Discussed in Thread: UCC28600, UCC28704, UCC28740
HI
There is a reference circuit 150W AC/DC with UCC28630
http://www.ti.com/lit/ug/tidub50b/tidub50b.pdf
Is there output accuracy data for over temperature(–10°C to 55°C) ?
There are Load regulation and Input regulation data, but could not find over temp data.
best regards K.Kanao