Other Parts Discussed in Thread: BQ34Z100
I am currently performing a learning cycle for the following battery pack:
LiFePO4 Battery, 15 in series, 3.2V nominal per cell, 40Ah capacity
After configuring the BQ34Z100-G1, I performed the following learning cycle:
1) Started with a full battery (relaxed for a few hours), IT enabled. After a few minutes, OCVTAKEN toggles high.
2) Discharged battery to terminate voltage, disconnected load. Allowed pack to relax until OCVTAKEN is set.
3) Charged battery until taper current is reached. FC bit is set. Disconnected charger from pack. BQ34Z100 goes into relax mode waiting for OCVAKEN to set.
It has been almost 36hrs but the OCVTAKEN flag is still low. I would like to ask what could be preventing the OCVTAKEN bit from toggling.
At this point the learned status is already at 05 and max error is 3%.
Attached is the gg and log file of the learning cycle. Thanks!
PS: I also tried the learning cycle where the process begins with a discharged battery but the same issue crops up.