This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5150-Q1: ISHUTDOWN(VOUT) and ISTANDBY(VOUT) under Vout=5V

Guru 29720 points
Part Number: LM5150-Q1

Hi Team,

My customer considers to use LM5150-Q1 for automotive application.
He wants to know ISHUTDOWN(VOUT) and ISTANDBY(VOUT) under Vout=5V as a reference.
Could you tell me these values if you have?



Best Regards,
Yaita / Japan disty

  • Hi
    The device cannot stay in the standby mode when the output voltage is 5V. The device will switch in order to regulate the output voltage if the output voltage is less than the regulation target. The VOUT pin shutdown IQ at 5V is typically 5uA~6uA.
    Regards,
    EL