Other Parts Discussed in Thread: GPCRB, , BQSTUDIO
Hello,
I have a fuel gauge BQ34Z100-G1, I have create a Optimized resistance temperature compensation parameters with the SLUUBD0 document. The battery is at 25.6V and when I reset the gauge, the remaining capacity and the RSOC have the coherent value. the RSOC is 25%. If I discharge or I charge the battery, the remaining capacity and the RSOC increment and decrement. after one day in relax for the battery with the battery voltage at 25.6V and the ambiant temperature are 20°C, We see the remaining capacity and the RSOC at 0 maybe the voltage is 25.6V. I join the GPCRB that I receive.
Thanks.gpcrb.rar