This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS60150: Current Limit Protection

Part Number: TPS60150


Hi

My Customer has question.

■Q1
Although the TPS 60150 has the Short Protection function,Do you also have Current limit Protection function?
Is it possible to understand that the threshold is 300 mA from Datasheet P10 Figure 6?

■Q2
After overcurrent or Short protection works, when the current value returns to the normal value, the output voltage returns to the steady value.
⇒With this understanding ok?

Best Regard

T Kishi

  • A1: According to the datasheet, it has a current limit as shown in Fig 6. 300mA is a typical value and we do not have characterization data to tell the tolerance in real circuit performance.

    A2: You understanding is right.