This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A6401-Q1: The abnormal waveform of nRST pin

Part Number: TPS7A6401-Q1

Hi,

Our customer used TPS7A6401-Q1 to convert 12V to 5V/300mA, but they encountered problems. When nWD_EN and WD pin keep low level, the waveform of nRST pin should be a low reset level periodically. However, actually,  the time of low level is very short, and then ramp up slowly. So, what reason may result in the abnormal waveform of nRST pin? If this waveform apply to the RST pin of MCU, can MCU reset normally? Thanks!

Note: The schematic as same as that of TPS7A6350, because it is pin to pin with TPS7A6401, and FB pin has connect correctly. The waveform of nRST pin as picture 2.