Hi, I used BQ25010RHLR in the past for my custom PCB.
Now, I'm using a Li-ion battery pack that is parallelly connected
and micro USB will be used to charge this battery.
This is the battery pack I'm using; take a look at the link. (summary: 3.7~4.2V, 18650 type, 4000mAh).
I'm going to use one packed battery per PCB. In the BQ25010's datasheet, it says
The integrated low-power high-efficiency dc-dc converter is designed to operate directly from a single-cell Li-Ion or Li-Pol battery pack
1. I don't know much about batteries. Is the aforementioned packed battery considered as a single-cell battery?
2. If I cannot use BQ25010 with this packed battery for USB charging, is there an alternative charging IC from TI I can use?
It will be great if that IC has a buck converter like the BQ25010 and capable of micro USB charging.