Good morning,
I am using this DCDC and I find some problems in the configuration of the feedback resistors.
If I want to configure Vout = 1.8V using the equation given in the datasheet Vout=0,8V*(1 R1/R2)
I get R2=100k, R1=125k. But in the datasheet it is suggested to use 124k. The same says the Webench simulation.
The same thing happens with Vout=1.2V:
I get from the equation R1=50k, R2=100k, and from webench R1=49.9k.
Is it the equation correct? Which values should I trust/use?
thank you very much,
regards
Leonardo