This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM337: LM337

Part Number: LM337

Hello,

I need a tunable voltage between -42V and -20V.

Can I use the LM337 negative LDO with, for example, an input of -45V while |VI-VO|< 40V ?

 Or, in any case -37V is the lower output voltage?

Thanks in advance,

Regards,

Stéphane