Other Parts Discussed in Thread: BQ25504
Input to the BQ25504 is an IXYS product. In the same size, it comes in either one cell KXOB22-12X1L or 3 cells. I have tried the single cell. It is agonizingly slow at charging a super cap of say 5F to 3.6V, even in full sun when the cell should be producing about 40mA at 0.5V. I calculate it should charge the capacitor is a few hours. Would I be better off using the 3 cell solar cell producing 14mA at 1.5V?
Maybe my calculations are wrong, or I have programmed BAT_OV wrong.