This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070: EXTERNAL CLOCK SYNC

Part Number: UCC28070


hello
i have a couple of question .
1. If I use external clock sync what is the maximum frequency range that i can achiev. For an example can i achiev 50% dither magnitude of fpwm.
2. And i work with 30kHZ fpwm can i work below 30kHz in the low line voltage , and can the ucc28070 controller handle with that. Or i should go to hihger PWM frequency.
3. I cant understand what is the value of ksync ( ramp reduction factor) it should be equal to 1 or somthing else.

Regards
ilia