Other Parts Discussed in Thread: TPS62740, BQ24092
Hello,
For a wearable device design we picked BQ25120 , but for First Prototype we need something which is Not DSBGA 0.4mm pitch package (Blind Via cost too high for first Proof of concept prototype).
Can you please suggest another single device solution which -
Allows charging from 5V source, for single cell, and includes Fuel gauge metering via I2C as well ?
(For the Switching-Regulator and Load-switch features, I have picked TPS62740 for prototype).
The BQ24092 as battery charger seems nice but it doesnt have Fuel gauge function.
Please suggest a suitable chip with: charging + fuel guage.
BTW: Please inform TI web team that all the Links on Battery Charger search page result in 404 / forbidden Fault -
try clicking any link on battery charge high-level filter page: http://www.ti.com/power-management/battery-management/charger-ic/overview.html
Error is -
Forbidden
Cannot serve request to /power-management/battery-management/charger-ic/products/ on this server
Thank you