This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq76PL455A-Q1: DAISY CHAIN bq76pl455a max. Cable lenght

Part Number: BQ76PL455A-Q1
Other Parts Discussed in Thread: BQ76PL455A

Hello,

i hope i can find some help for my Project. It´s about a controlling 144 battery cells in series. The datasheet says that the bq76pl455a can be daisy chained up to 16 devices in a row. Because of package reasons I have to use 12 Devices in a row ( daisy chain).

Now my question:


Is there a cable lenght limit for connecting all Devices as daisy chain ?

I calculated that I will be about 3m cable length, divided up in 6 parts with 0,5m.

Thank you !