Other Parts Discussed in Thread: BQSTUDIO
Hi,
I'm using a B35100 in "Coulomb Accumulation" mode with a multi-cell (4 x Li/SOCl2) configuration. The calibration is done ( current and voltage ).
I'm trying to understand how to get the unit of the coulomb counter.
In the TRM § 11.1 the unit of this data is Ah, but for example with a fix 300 mA Load during 10 minutes the delta off the AccumulatedCapacity data is: 4900 .
Each time I test it the ratio is almost constant: (600*300) / 4900 = 3.6
What is this value? Is it possible to get it from the DF data?
Gwendal Le Gall
PS:
This is a partial dump of the DF data memory (calibration part):
address,name,value
4000 , CC Gain F4 ,7B3EB0E6
4004 , CC Delta F4 ,8F58F6C3
4008 , CC Offset I2 ,FA88
400A , AD I Offset I2 ,004C
400C , Board Offset I1 ,F8
400D , Int Temp Offset I1 ,00
400E , Ext Temp Offset I1 ,00
400F , Pack V Offset I1 ,AA
4010 , VIN Gain U2 ,9FC9
4012 , Int Coeff 1 I2 ,0000
4014 , Int Coeff 2 I2 ,0000
4016 , Int Coeff 3 I2 ,CFDC
4018 , Int Coeff 4 I2 ,17F3
401A , Int Min AD I2 ,0000
401C , Int Max Temp I2 ,17F3
401E , Ext Coef 1 I2 ,51F6
4020 , Ext Coef 2 I2 ,C9F4
4022 , Ext Coef 3 I2 ,1452
4024 , Ext Coef 4 I2 ,0921
4026 , Ext rc0 I2 ,326D
4028 , Vcomp Coeff 1 I2 ,0000
402A , Vcomp Coeff 2 I2 ,3A36
402C , Vcomp Coeff 3 I2 ,FD91
402E , Vcomp Coeff 4 I2 ,0025
4030 , Vcomp Input Multiplier U1 ,30
4031 , Vcomp Output Divisor I2 ,0100
4033 , Filter U1 ,EF