Are Bit 1 and Bit 0 of Learned Status reversed on Page 20 of the manual (SLUSBZ5B)? It states:
QMax (Bit 3): QMax updates in the field.
0 = QMax has not been updated in the field.
1 = QMax updated in the field.
ITEN (Bit 2): IT enable
0 = IT is disabled.
1 = IT is enabled.
CF1, CF0 (Bit 1–0): QMax Status
0,0 = Battery is OK.
0,1 = QMax is first updated in the learning cycle.
Or are Bit 1-0 for Qmax Status displaying the least significant bit first? I typically get 0x02 before IT Enable and 0x06 after IT Enable.
With regards to Bit 3, what is considered "updated in the field". Is this updated after IT Enable, after being Sealed???
What would the normal progression be for Learned Status?