This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there a MIC5205 equivalent in TPS series?

Other Parts Discussed in Thread: LP2985, TLV713, TLV760

Hello,

MIC5205 is a 3.3V LDO with EN, and 0.15A output. Is there a TPS equivalent for this?

I have been using TPS73633 which is good to 0.4A - but it is costly comprared to a MIC5205? So is there a cost effective ti part equivalent to this ldo?

Also, sometimes I need to switch on and off the power busses. Is there a ti part that for example takes 3V3 from the output of a TPS73633 and depending on an EN pin outputs a 0.15A 3V3 from output pin? like a switch?

Best Regards,

C.