This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMB1428Q: emb1428,vgs=36v

Part Number: EMB1428Q

HI

I tested a board,PLUS Vgs>36V.This is an unusual situation.

correct vgs=12V.

plus-minus Voltage 47V.

FETmos is ok.

  • Hi User,
    The Vgs >36V sounds abnormal. The EMB1428 should only be capable of 14V maximum output gate - source, normally 12V as you indicate, and a FET should turn on as a follower limiting Vgs if the source reference is lost. You might check for missing solder on some pin or a pin shorted. If the condition continues it seems the part must be damaged.