Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
hello
I try to simulate 18kw full bridge with 400V input and 450V output.
Output current 45A to 1mA. I tried to do that with the EVM sim model but with no succeed. I cant make the output voltage up to 450V. Its stays at 18V max.
I want to use it in battery charger. I already made the output current to change but now i want to simulate with 450V output voltage.
Do you have any suggestions why i can't reach the output voltage.
regards
ilia