This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: UCD9090A Re-sequence operation does not work

Part Number: UCD9090A


Hi,

I have a board with the UCD9090A sequencer that successfully sequence on and off the rails when I power the card on and off.

When I test a failure scenario that should sequence off the rails and sequence them back (re-sequence) the sequence off function ok but the device does not sequence on again.

I followed the instructions on "UCD90xxx Sequencer and System Health Controller PMBus Command Reference" document (slvu352f) section 10.25.2 "Re-Sequence" but still the re-sequence operation does not work.

I have 10 monitor supplies and a GPI that control the sequence on and off with the correct dependencies.

The setting of register MFR_SPECIFIC_44 "Miscellaneous Configuration Byte" is 0x88 which configures the sequencer to Resequence Continuously.

I can send any information that is necessary.

Please advice,

Best Regards,

Yossi