This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: VRECHG can be setup?

Part Number: BQ24610

Hi TI'ers,

I am interested in BQ24610 and i have some doubts when i look through the datasheet.

I didn't find the definition and range of VRECHG, only know in case of Vcc<VRECHG, the device will open the charging cycle.

I  eagerly want to know if VRECHG can be set up by myself. If not, could you tell me the definition and range ?

Thanks & Best Regards

  • Please refer to the electrical characteristics table on page 8.
    When the VFB voltage falls 50mV below 2.1V (regulation voltage), recharge starts. For example, if the battery regulation voltage is set to 8.4V, then the recharge threshold is 8.2V.