This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS548A20: request schematic review (TPS548A20RVER / TPS54623RHLR / TPS563219ADDFR )

Part Number: TPS548A20


Hi,

We ask TI to review whether below parts are working properly.

Power_Review_sch.pdf

It is based on the following criteria.

input :  12V

output :

  1. +3.3V_SFP : 12A

  2. +1.0V (except)

  3. +3.3V : 5A

  4. +1.5V : 2A

  5. +1.8V : 1.5A

  6. +1.2V : 1A

  7. +1.05V : 5.6A

  8. +3.3V_OCXO : 1A

 

thanks,

TS

  • Since these parts are supported by different groups, you should make an individual post for each circuit.  Also for each circuit, can yo post your design inputs, your design care abouts (transient response, efficiency , size, etc) and the method that you used to determine the external passive components (webench or some other methosd such as a spreadsheet)?