Hello,
Are there any recommended solution of the following requirement?
We could use transformer.
Vin = -15V
Vout = +5V
Iout=1A
Vin = -15V
Vout = -90V
Iout=10mA
Best Regards,
Ryuji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Are there any recommended solution of the following requirement?
We could use transformer.
Vin = -15V
Vout = +5V
Iout=1A
Vin = -15V
Vout = -90V
Iout=10mA
Best Regards,
Ryuji
Hi Ryuji,
For -15V to 5V/1A, take a look at PMP4742 http://www.ti.com/tool/PMP4742?keyMatch=null&tisearch=tidesigns-power There are several circuits on this design, but the TPS40210 plus TL431A is a way to boost a -12V input to a 12V output. This is the architecture that you would need.
For -15V to -90V/10mA, you can use a boost architecture like shown in PMP4589 http://www.ti.com/tool/PMP4589 and leverage a doubler or tripler like shown in PMP8956 http://www.ti.com/tool/PMP8956?keyMatch=null&tisearch=tidesigns-power The doubler or tripler will help lower the duty cycle of the boost.
Ryan