Hi ,
I am develop an LM5088 application. Input voltage is 7-60Vdc. Output is 5V 5A. The problem is; When there is no load, output voltage continuously changes in 3-4V range. Also, I hear the coil voice.
I am using 8.2uH coil and double N-FET BSC123N08 . fw=275Khz. I saw suggestions about Cvcc and Cboot. I decreased/increased the capasitor values. There is a change, but when Vcc:1uF and Vboot: 100n with load,Vinmin=6V, when i make a change,Vinmin=7.3V with load.
What can i do?