This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62090: min/max switching frequency

Guru 20090 points
Part Number: TLV62090


Hello,

Could you please let me know the min/max switching frequency at heavy load?
According to the datasheet figure 3~6 ,  is the fsw(min) about 1.1MHz and fsw(max) about 1.5MHz?

Best Regards,
Ryuji

  • Hello Ryuji,

    it's a pleasure to support you. Figure 3 to 8 in the datasheet show the switching frequency dependency with the load current Iout and input voltage Vin and output voltage Vout. The combination of these 3 conditions establish the switching frequency regime. Furthermore also the passives influence the switching frequency, so keep in mind that the pictures refer to this configuration: L = 1 µH, Cout = 22 µF

    Hence, you should identify the graph closer to your case's operating condition and refer to that one to estimate the switching frequency. Example:

    Vout=1.8V ; Vin= 2.8V  : Iout=1A to 3A -> figure 3 fits -> fmax=1.5MHz circa ; fmin=1.25 MHz circa

    Enjoy your design!

    Best Regards,

    Emmanuel

  • Hello Emmanuel san,

    I appreciate your supply.
    Could you please let me know the switching frequency vs. temperature data?
    Our customer would like to know the frequency variation by temperature.
    I appreciate it if you share the data.

    Best Regards,
    Ryuji
  • Hi Emmanuel san,

    I got additional question.

    Could you please let me know the part to part difference of switching frequency on same condition?

    Best Regards,
    Ryuji

  • Hello Ryuji,

    TLV62090 has DCS control topology, hence the switching frequency variation depends on input voltage, load current, output voltage and output filter as well. Due to all these variables playing their role, we are not able to gather switching frequency variations over temperature and process.

    Best regards,
    Emmanuel