Hi,
Could you tell me the information about TPS543C20?
Is there the data on load transient characteristics under the following conditions when using TPS543C20EVM-869?
【condition】
Vin: 10 V or 12 V
Vout: 0.95 V or 1.05 V
Iout: 50A to 60A (the slew rate is 16 A/us.)
Also, our custormer's request is that the load transient falls within ± 20 mV.
What is the value of Cout to achieve this?
Best Regards,
Yuto Sakai