Hi,
I am using BQ34z100-g1 with an 8s2p LiFePO4 battery.
I have charge the battery to full at 23ºC and the the FCC has raised from 6400 (=designCapacity) to 6613mAh.
After that I have introduce the battery in a climate room and set -20ºC. The FCC has dropped to 6075mAh. Then I have started a discontinuous dicharge at C/3.
Now, the battery is at 75% SoC with the next parameters
- FCC=6075 mAh
- RC = 4572 mAh
- TRC = 3852 mAh
- TFCC = 5233 mAh
- SoH = 100%
I have some doubts about them:
1. Why is SoH = 100%. I have read SoH is FCC/designCapacity() but in this case this is not correct.
2. What does the parameter SOH_DISP do? Is it necessary to read a real SoH?
3. If TRC is 3852 mAh (and is lower than TFCC), how can be RC 4572 mAh?
Thank you very much in advance,