This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: EEPROM Configuration

Part Number: LP8860-Q1


Hi,

We got a question from the customer about LP8860-Q1.
Could you help us?

[Question]
They are considering using LP8860-Q1 under the following condition.

 Vin=7 to 16V
 Vf=32V
 If=90mA/ch *4ch
 fsw=2.2MHz

They refered to the summary of LP8860 EEPROM configurations, but they couldn't find the correct setting for them. So they are considering burning EEPROM with thier requirement in their production line. Are there any concerns to burn EEPROM in their production line?

Best Regards,
tateo