This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17381F4: Do we have the test circuit for the VDS of the CSD17381

Part Number: CSD17381F4


Hi team,

My customer want to check how we test the VDS of the CSD17381 from the datasheet?

Thanks.

BR

Frank

  • Frank,
    We do have an EVM we are working on specifically for testing these very small devices. Th plan is to put 6 different N-Channel devices on it, though I am not exactly sure of the time table for release. I would reach out to my colleague Kevin O'Connell for details.

    Why do they need to test VDS? This is a parameter we guarantee as it is tested in production.
  • I think I misread your first post - I think you were just asking about how we test the device, not for a board to test in themselves.

    We test every device in production. The conditions of how we test are specified in the electrical characteristics of the datasheet.

    Basically, the max voltage is applied to the device (in this case 30V) at room temperature (Ta = 25deg). If the device's breakdown is exceeded, it will avalanche, and the device will fail the test, and be discarded.