This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28730-Q1: UCC28730-Q1

Part Number: UCC28730-Q1
Other Parts Discussed in Thread: UCC28730,

Helo TI forum,

I have some problem to solve. Has far I have read the flayback converters uses a "transformer" to convert DC to DC with a maixm input voltage of 700V, But 

Wich is the minimal voltage at the output?. The problem that I have is that I have a 700V DC and I have to convert it to 1500V with 60A at the output. Yes I know is hard, but

all reference that I have read didn't clear anything to me. There are anywhay to convert 700VDC to 1500VDC with 60A with TI drivers?

Thanks