This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31707: AGND and PGND

Part Number: LMZ31707


Can someone please confirm that AGND and PGND are tired together inside the device? Thus I should not connect them on the PCB, right?   

I think that's what the datasheet says, but I just want someone to confirm. As this is my first time using this type of module, so find it odd that the AGND should just be by itself a copper shape on the PCB.

Does it hurt something if i put down a zero ohm (but not install the 0ohm) connect between AGND and PGND.

Thanks.