I tested a boost board loop response using LM5122 conference with TIDA-PMP20093 and the bode as shown below. I found the issue that the phase become very large and the mag start increase when the frequency is 5MHz. I wonder what's the reason of this issue and how to solve it.
The spec of the boost board are: Vin=14.4V Vout=24V. Because the limit of input range of Loop Analyzer(15Vmax), I changed the Vin=8.5V &Vout=14.2V & Iout=2A. The schematic as below shown.