Other Parts Discussed in Thread: BQ76200, , BQ78350, BQSTUDIO
Hello to TI Team ,
I use 13S connection cells with bq7694001 with 78350-r1 and bq76200 driver ( exactly according to TI design notes on TIDA -00792) .
The problem I see is recovery from ShutDown .
1. After I send twice Shut Down Command it enters to shutdown mode , as expected . ( Current consumption PCB < 10uA , no COMMunication , Output Voltage = 0V).
2. Now i want recover the battery from ShutDown , I set Voltage on TS1 pin more than VBOOT (according to Spec ) and i see that ( PCB current consumption back to normal ~1mA , Com operated and Regoutpin=2.5V) , but data that 78350-r1 receive from AFE totally wrong ( Temp ~200C , cells ~50mV each cell) picture attached . As i understand AFE internal block not proper wake up from Shutdown .
I tested shut down recovery problem on real parameters (without command) it has recovery problem too !
2.1 The only thing that back to show normal parameters after par 2 problem is DISCONNECTION OF CELLS , CONNECTION BACK and WAKE UP !
B.R
Alexander Burtakov