This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710: Thermal dissipation

Part Number: LMZ31710

Hi,


Im I designing an stand alone system WITHOUT any active cooling, so, thermal dissipation is a key paramenter. We are thinking in using dissipators attached to the main heating producers of the board.

For this project, I have selected DC-DC LMZ31710. So, my questions are related to this component.

Which is the best way to cool down this component ( without any active system ? )

- with a heatsink on top of the package

- with a heatsink attached to the bottom of the board, to GND PAD of LMZ31710 ?

- other ??


All information that you could give us about thermal dissipation of this component is welcomed.


Regards

Jordi

  • Hi Jordi,

    The LMZ31710 has several PH pins(Phase switch node) that can be connected to one another for thermal relief. The recommended layout considerations in the datasheet provides common practices for optimizing thermal performance of the part with the need for active cooling. Power path traces should be wider than signal on the PCB layout. If needed adding a heatsink to the top of the package will also aid in thermal dissipation. 

    Regards,

    Jimmy 

  • The best recommendation for drawing heat from the package is to add extra copper area on the PCB for the Vout, PH and PGND pads and layers.