Other Parts Discussed in Thread: TPS82130
Hi,
Could you give me advice.
Can I use TPS 63700 under the following conditions of use?
Vin 3.3 V
Vout -3.4 V
Iout 200 mA
Please tell us from the viewpoint of current value and duty.
I do not have a description of the efficiency curve that is close to the input / output condition and there is no formula for calculating Duty, so I want to check it.
Best Regards,
Yuto Sakai