This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90240: Can VREFA+ and VREFA- pins be left floating if internal reference is being used.

Part Number: UCD90240


The datasheet says that the use of these 2 pins are optional, but when not using them is it alright to leave them floating when using the internal voltage reference? None of the reference circuits show a case in which only the internal reference is used.