Other Parts Discussed in Thread: BQ34Z100, BQ34110
I have to make a 6S BMS for Li-ion.
Can i connect in series two 3S packs using bq20z95 on each 3S pack.
On SMBus only current has to be read via lowest bq20z95.
1. While discharge, i think this system will work ok, as if either one is off, there will be no voltage output.
2. Whle on charging, problem will arise, if lower one is off, and charger is connected, system will never get turn on.
Is there any solution to it?
3. any other downside?
4. is there any other 6S complete solution like bq20z95, which has all features of bq20z95