This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51220A: About EN threshold

Part Number: TPS51220A

Hi,

Let me discuss about TPS51220A EN threshold.
The data sheet has the following description.



When considering hysteresis, is it correct with the following understanding?
MIN:0.7V (0.8-0.1V)
TYP:0.8V (1-0.2V)
MAX:0.9V (1.2-0.3V)

Customers want to know the exact threshold of EN.
Could you tell me how to interpret hysteresis?

Best Regards,
Yusuke/Japan Disty