I'm working on a project using the TPS92691. It is fairly high power with vin 10 - 30 V dc, and a Vf string of LEDs of around 60vDC, driven at 1A.
I am having issues with driving with PWM at lower input voltages - esentially I am hitting the current limit causing flicker, on the rising edge of the PWM signal. The image shows the voltage across the Fet current sense resistor (0.03Ohms). The problem is the initial peak ramp up of the current through the inductor seems to be higher than it should, before the switcher starts cycling again?
The data sheet states:
"On the rising edge of the PWM input voltage (VPWM > 2.5 V), the GATE and DDRV outputs are enabled to ramp the inductor current to the previous steady-state value. The
COMP pin is connected and the error amplifier and oscillator are enabled only when the switch current sense voltage VIS exceeds the COMP voltage, VCOMP, thus immediately forcing the converter into steady-state
operation with minimum LED current overshoot."
However this does not seem to be happening, and does not seem correct as the COMP pin voltage is ~2V, so Vis will never get that high?.
Any suggestions other than increasing the current limit (it is now currently ~17A, which is already more than the saturaton current of the indcutor ~12A).