Other Parts Discussed in Thread: TPS65263
The customer is considering power supply for LPDDR 4 with automotive application.
I would like to propose it with TI's power supply products.
I understand that the power supply necessary for LPDDR 4 is the following power supply.
 ・VDDQ:1.1V
 ・VDD1:1.8V
 ・VDD2:1.8V
In addition, this input voltage is 5 V specification.
Q1.
In this case, is it possible to use the TPS65263-Q1 as the LPDDR4 power supply?
*Information on the power supply of in-vehicle parts that supports LPDDR 4 is required.
-Harukawa