This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23625: LMR23625CFDDA fails to start up with a capacitive load

Part Number: LMR23625
Other Parts Discussed in Thread: LM73605

I've got a 7V 2.5A PSU design on one PCB that is used to power another PCB in the same unit.

The problem is that the PSU will not start-up as the other board is a high capacitive load - the other board has a 16V 2200uF input capacitor on it. This board can not be changed.

I've tested start up of the supply with a resistor load box up to 2.5A and it starts up perfectly, it just seems to be the capacitive load that is upsetting it.

Here is the schematic: (The snubber network is not fitted)

PCB layout:

Is there anything that can be done to slow down the start-up or make the part happy about the capacitive load?

Thanks,

Graham