Dear All,
Its a matter of very urgency, so your would be very much appriciated. I have 2 BQ76PL455 EVM's which i need to use for stack communication. But one of the board is not at all waking up. The following voltages are measured:
- VIO is 5.16V
- VDIG is 0V
- V5VAO is 4.49V
- TOP is 57V
- TX is 5.15V
- RX is 5.16V
- WAKEUP is 0V
- Q17 ZXTN4004K NPN Transistor Base is measuring 0.44V
- Q17 ZXTN4004K NPN Transistor Emitter is measuring 0.V
- Q17 ZXTN4004K NPN Transistor Collector is measuring 57V
The LED D22 does not lit up at all and I have no idea what else to check can you please help me resolve the issue ?
Kind Regards
Vikram Jain