Dear TI member,
I use TI BQ24295 EVM (BQ24295EVM-549) to test.
Condition: No Battery, use DC Electronic Load and connect to sys pin, set load = 0.4A, turn on.
After providing the 5V to VBUS, VSYS will power on then power off, and power on afterward.
BUT sys pin always is 1.9V~2V,instead of normal voltage 3.6V.
The IOUT peak current just only 0.5A, I think not reach the current limit protection.
Does it touch others protection functions?