Hello,
I want to use TPS54361.
I want to work at the highest possible frequency!
What is the maximum frequency I can reach with the component ,while the input voltage is 60V and the load current is the max 3.5A output voltage is 5.5V and 3.3V.
Thanks