This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: Can I use 2 BQ76940 support 24-Series cell application?

Part Number: BQ76940
Other Parts Discussed in Thread: BQ76930, TIDA-01093, BQ34110, BQ34Z100-G1

Hi sir/madam,

I looked through the website and found that Ti has a reference design of 2 BQ76930 to support maximum 20-series cell application, and the situation of mine is maximum 27-Series cell application(type 24-Series), Can i use 2 BQ76940 to meet my design like  [ http://www.ti.com/lit/ug/tiduc43a/tiduc43a.pdf ]?

If yes, could you send me a reference design document?

If no, could you support a better solution of gas guage?

Thanks & Best Regards

Jenny

  • Hi Jenny,
    The same approach could be used for up to 30 cells with the bq76940. Be sure to adjust the component ratings where needed. See TIDA-01093 for reference documents.
    For a gauge consider the bq34z100-G1 or bq34110